ACTION#.CONDITION
Description
This keyword defines the condition to test the action source for. If the value is 0 (always), then no test is performed and the condition always passes.
The available values of this parameter depend on the value of ACTION#.SOURCE. If the source is changed, the available range may be updated and the condition will be reset to default. Available conditions are:
| Value | Description |
|---|---|
| 0 | Always passes |
| 1 | Is false |
| 2 | Is true |
| 3 | Less than |
| 4 | Greater than |
| 5 | Rising Edge |
| 6 | Falling Edge |
| 7 | Rises above threshold |
| 8 | Falls below threshold |
| 9 | Rising Edge (triggers on high at start) |
| 10 | Falling Edge (triggers on low at start) |
| 11 | Is Equal To |
| 12 | Becomes Equal To |
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
Depends on ACTION#.SOURCE |
|
Default Value |
0 (always) |
|
Data Type |
Integer |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.